Solid Edge Geometry Type Library
GetParamOnFace Method
Specifies the number of points to be evaluated.
Returns the parametric point.
Returns True if the input parametric point is unambiguously inside the trimmed region.
Description
Determines whether specified parameter lies within the trimmed region defined by the boundaries on the surface.
Syntax
Visual Basic
Public Sub GetParamOnFace( _
   ByVal NumParams As Long, _
   ByRef Params() As Double, _
   ByRef OnFace() As Boolean _
) 
Parameters
NumParams
Specifies the number of points to be evaluated.
Params
Returns the parametric point.
OnFace
Returns True if the input parametric point is unambiguously inside the trimmed region.
Remarks
GetParamFace returns True when the parametric point lies unambiguously within this trimmed region. GetParamFace returns False if the parameter is inside a hole or on a curve that defines the boundary.
Example
Private Sub Form_Load()
    Dim objApp As solidedgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objFace As solidedgegeometry.Face
    Dim dblParam(1 To 4) As Double
    Dim bOnFace(1 To 2) As Boolean
    Const TESTFILE = "T:\vbtests\testcases\HalfCyl.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the testfile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting the body object of the model
    Set objBody = objDoc.Models(1).Body
    ' getting a particular face from the collection of faces on the body
    Set objFace = objBody.Faces(FaceType:=igQueryAll).Item(2)
    ' checking whether a point represented in parametric form is on a face or not
    dblParam(1) = PI
    dblParam(2) = 0.05
    dblParam(3) = 1
    dblParam(4) = 1
    Call objFace.GetParamOnFace(NumParams:=2, Params:=dblParam, OnFace:=bOnFace)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFace = Nothing
End Sub
See Also

Face Object  | Face Members