Solid Edge Geometry Type Library
GetBSpline2dInfo Method
Returns the order of the referenced BSpline.
Returns the number of poles for the referenced curve.
Returns the number of knots for the referenced curve.
Returns True if the curve is rational (that is, a weight is assigned to every pole).
Returns True if the referenced curve is closed
Returns True if the referenced curve is periodic.
Description
Returns overall information related to the referenced B-Spline object.
Syntax
Visual Basic
Public Sub GetBSpline2dInfo( _
   ByRef Order As Long, _
   ByRef NumPoles As Long, _
   ByRef NumKnots As Long, _
   ByRef Rational As Boolean, _
   ByRef Closed As Boolean, _
   ByRef Periodic As Boolean _
) 
Parameters
Order
Returns the order of the referenced BSpline.
NumPoles
Returns the number of poles for the referenced curve.
NumKnots
Returns the number of knots for the referenced curve.
Rational
Returns True if the curve is rational (that is, a weight is assigned to every pole).
Closed
Returns True if the referenced curve is closed
Periodic
Returns True if the referenced curve is periodic.
Remarks
Use this method to determine the amount of memory needed to obtain the variable length information that fully defines the object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objPBCurve As solidedgegeometry.ParamBSplineCurve
    Dim lngOrder As Long
    Dim lngNumPoles As Long
    Dim lngNumKnots As Long
    Dim bRational As Boolean
    Dim bClosed As Boolean
    Dim bPeriodic As Boolean
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the test case file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a ParamBSplineCurve from the test case
    Set objPBCurve = objDoc.Models(1).Body.Shells(1).Faces(1).Loops(1).EdgeUses(1).Geometry
    ' getting the BSpline2dInfo for the ParamBSplineCurve object
    Call objPBCurve.GetBSpline2dInfo(Order:=lngOrder, NumPoles:=lngNumPoles, NumKnots:=lngNumKnots, _
                                     Rational:=bRational, Closed:=bClosed, Periodic:=bPeriodic)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPBCurve = Nothing
End Sub
See Also

ParamBSplineCurve Object  | ParamBSplineCurve Members