Private Sub Form_Load()
Dim objApp As SolidEdgeframework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objPBCurve As solidedgegeometry.ParamBSplineCurve
Dim bIsClosed As Boolean
Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
Call objDoc.Close
' opening the test case file
Set objDoc = objApp.Documents.Open(TESTFILE)
' getting a ParamBSplineCurve from the test case
Set objPBCurve = objDoc.Models(1).Body.Shells(1).Faces(1).Loops(1).EdgeUses(1).Geometry
' checking whether the BSpline curve is closed
bIsClosed = objPBCurve.GetIsClosed
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objPBCurve = Nothing
End Sub