Solid Edge Geometry Type Library
Parent Property
Description
Returns the parent object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Parent As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objPBCParent As solidedgegeometry.EdgeUse
    Dim objEdgeUse As solidedgegeometry.EdgeUse
    Dim objPBCurve As solidedgegeometry.ParamBSplineCurve
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the test case file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting an EdgeUse object from the test case
    Set objEdgeUse = objDoc.Models(1).Body.Shells(1).Faces(1).Loops(1).EdgeUses(1)
    ' getting the ParamBSplineCurve object
    Set objPBCurve = objEdgeUse.Geometry
    ' getting the Parent object of the ParamBSplineCurve object
    Set objPBCParent = objPBCurve.Parent
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPBCParent = Nothing
    Set objEdgeUse = Nothing
    Set objPBCurve = Nothing
End Sub
See Also

ParamBSplineCurve Object  | ParamBSplineCurve Members