Solid Edge Part Type Library
BlueSurf Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method DropParentsRemoves associative connection with parents, so that it can not edited or recomputed.
Public Method ExactRangeThis method sets the exact range parameters for the referenced object.
Public Method GetCrossSections
Public Method GetEndGuideTangentData
Public Method GetEndSectionTangentData
Public Method GetGuides
Public Method GetStartGuideTangentData
Public Method GetStartSectionTangentData
Public Method GetStatusExReturns the status of the specified object.
Public Method InsertSketch
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetCrossSectionsThis method sets the cross sections associated with the referenced feature object.
Public Method SetEndGuideTangentData
Public Method SetEndSectionTangentData
Public Method SetGuides
Public Method SetOriginsThis method sets the origin points for the referenced object.
Public Method SetStartGuideTangentData
Public Method SetStartSectionTangentData
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property EndCapsStatusSets and returns the end caps status for the referenced object.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property GuideEndTangentType
Public Property GuideStartTangentType
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property ModelingModeTypeReturns the modeling mode of the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property Periodic
Public Property SectionEndTangentType
Public Property SectionStartTangentType
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

BlueSurf Object