Solid Edge Part Type Library
Faces Property
Description
Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Faces( _
   ByVal FaceType As FeatureTopologyQueryTypeConstants _
) As Object
Parameters
FaceType
ValueDescription
igQueryAllFeature Topology Query Type - All
igQueryConeFeature Topology Query Type - Cone
igQueryCylinderFeature Topology Query Type - Cylinder
igQueryEllipseFeature Topology Query Type - Ellipse
igQueryPlaneFeature Topology Query Type - Plane
igQueryRoundableFeature Topology Query Type - Roundable
igQuerySphereFeature Topology Query Type - Sphere
igQuerySplineFeature Topology Query Type - Spline
igQueryStraightFeature Topology Query Type - Straight
igQueryTorusFeature Topology Query Type - Torus
Remarks
The result of the Faces property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. By default, the Faces property returns all faces for the object. The topology collection can be restricted to a specified type of face by supplying a value (from the FeatureTopologyQueryTypeConstants constant set) for the FaceType argument for the feature objects only. For example, this property can be set to return all faces that are spheres.
See Also

BlueSurf Object  | BlueSurf Members