Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
CoordinateSystem | Sets or Retrieves CoordinateSystem collection. |
CopyColors | This read-write Boolean property specifies whether colors are copied for the referenced CopyConstruction object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
FamilyOfPartsMember | Specifies whether or not the referenced object is a Family of Parts member. |
FileName | Sets and Returns the file name of the referenced document. |
IncludeConstructionCurveBodies | This read-write Boolean property specifies whether construction curve bodies are included for the referenced CopyConstruction object. |
IncludeConstructionSolidBodies | This read-write Boolean property specifies whether construction solid bodies are included for the referenced CopyConstruction object. |
IncludeConstructionSurfaceBodies | This read-write Boolean property specifies whether construction surface bodies are included for the referenced CopyConstruction object. |
IncludeDesignBody | This read-write Boolean property specifies whether the design body is included for the referenced CopyConstruction object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsBroken | Returns the broken status of object |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |