Solid Edge Part Type Library
SetIncludeBodies Method
Specifies the number of include bodies. If NumberOfIncludeBodies is 0, then IncludeBodies is ignored.
Specifies the include bodies. IncludeBodies must be an array of valid body objects if NumberOfIncludeBodies is not 0.
Description
Sets the scale of the referenced object.
Syntax
Visual Basic
Public Sub SetIncludeBodies( _
   ByVal NumberOfIncludeBodies As Long, _
   Optional ByVal IncludeBodies As Variant _
) 
Parameters
NumberOfIncludeBodies
Specifies the number of include bodies. If NumberOfIncludeBodies is 0, then IncludeBodies is ignored.
IncludeBodies
Specifies the include bodies. IncludeBodies must be an array of valid body objects if NumberOfIncludeBodies is not 0.
See Also

CopyConstruction Object  | CopyConstruction Members