Solid Edge Part Type Library
Hole2d Object
Members 
Description
Used to define the centers of holes on a profile that is used to define a Hole object.
Object Model
Hole2d ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Remarks
The Hole2d object should be the only 2-D object placed on a profile that will be used with a Hole object. The Hole2d object defines the center of the hole; an associated HoleData object defines the other attributes for the hole.
See Also

Hole2d Members