Delete | Deletes the referenced object. |
Duplicate | Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original. |
GetCenterPoint | Returns the point that is the center of the referenced object. |
GetKeyPoint | Returns information about a specified key point. |
Mirror | Copies the referenced object about an axis. |
Move | Moves the referenced object. |
Range | Returns the high and low range values for the referenced object. |
Rotate | Rotates the referenced object about the point specified by the angle in radians. |
Scale | Scales the referenced object by a specified factor. |
Select | Selects the referenced object in the active window. |
SetCenterPoint | Relocates the center point of the specified object. |
SetKeyPoint | Sets the position for a specified key point. |