Solid Edge Part Type Library
TaperLValue Property
Collapse All
Expand All
Solid Edge Part Type Library
>
HoleData Object
: TaperLValue Property
Description
Specifies the value to be applied to the hole Length for the referenced HoleData object.
Property type
Read-write property
Syntax
Visual Basic
Public Property TaperLValue As Double
Remarks
This value is used when the taper for a hole is to be calculated as a ratio between the Length (depth) and the Radius.
See Also
HoleData Object
|
HoleData Members