Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BottomAngle | Sets and returns the angle of the bottom of a finite hole. |
CounterboreDepth | Sets and returns the depth of the counterbore for an associated Hole object. |
CounterboreDiameter | Sets and returns the diameter of the counterbore for an associated Hole object. |
CounterboreProfileLocationType | Sets or returns the location of the counterbore profile for an associated Hole object by way of the referenced HoleData object. |
CountersinkAngle | Sets and returns the angle of the countersink for an associated Hole object. |
CountersinkDiameter | Sets and returns the diameter of the countersink for an associated Hole object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Fit | Sets and returns the Hole fit. |
HeadClearance | Sets and returns the head clearance |
HoleDiameter | Sets and returns the diameter of an associated Hole object. |
HoleType | Sets and returns the type of hole. |
InsideEffectiveThreadLength | Sets and returns the effective thread length associated with the inner diameter. |
InternalThreadDescription | Sets and returns the description associated with the internal diameter of the tapered thread. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
OutsideEffectiveThreadLength | Sets and returns the effective thread length associated with the outer diameter. |
Parent | Returns the parent object for the referenced object. |
Size | Sets and returns the Hole size. |
Standard | Sets and returns the database used for standardized Hole data. |
SubType | Sets and returns the Hole subtype. |
SystemName | This read-only String property returns the system name for the referenced object. |
Taper | Sets and returns the taper type. |
TaperDimType | Specifies whether the Taper dimension is to be specified from the top or the bottom for the referenced HoleData object. |
TaperLValue | Specifies the value to be applied to the hole Length for the referenced HoleData object. |
TaperMethod | Sets and returns the taper definition through the referenced HoleData object. |
TaperRValue | Specifies the value to be applied to the hole Radius for the referenced HoleData object. |
ThreadDataByDescription | Sets and returns thread data by description. |
ThreadDepth | Sets and returns the depth of a thread. |
ThreadDepthMethod | Sets and returns the method in which a thread is defined. |
ThreadDescription | Sets and returns the description of the thread. |
ThreadDiameterOption | Sets and returns the Thread diameter option. |
ThreadExternalDiameter | Sets and returns the external diameter of the thread for an associated Hole object. |
ThreadHeight | Sets and returns the thread height. |
ThreadMinorDiameter | Sets and returns the minor diameter of the thread for an associated Hole object. |
ThreadNominalDiameter | Sets and returns the nominal diameter of the thread for an associated Hole object. |
ThreadSetting | Sets and returns the thread setting type. |
ThreadTapDrillDiameter | Sets and returns the Tap Drill diameter. |
ThreadTaperAngle | Sets and returns the taper for the threads. |
TreatmentType | Sets and returns the type of treatment for the referenced object. |
Units | Sets and returns the units in which the line width is defined. |
VBottomDimType | Specifies where dimensions are calculated for the referenced HoleData object when the TaperMethod is set to igVShaped. |