Solid Edge Part Type Library
TaperRValue Property
Description
Specifies the value to be applied to the hole Radius for the referenced HoleData object.
Property type
Read-write property
Syntax
Visual Basic
Public Property TaperRValue As Double
Remarks
This value is used when the taper for a hole is to be calculated as a ratio between the Length (depth) and the Radius.
See Also

HoleData Object  | HoleData Members