Solid Edge Part Type Library
ThreadDataByDescription Property
Description
Sets and returns thread data by description.
Property type
Write-only property
Syntax
Visual Basic
Public Property ThreadDataByDescription 
Remarks
The property reads the existing feature measurement type and searches only for that type in holes.txt. Therefore, if the existing feature is in English units and a string corresponding to a metric entry in holes.txt is passed, it fails. However, if you suspect a unit mismatch, you can specify unit type with HoleData.Units and force it to work.
See Also

HoleData Object  | HoleData Members