Solid Edge Part Type Library
Arcs2d Property
Description
Returns the Arcs2d collection object for the referenced Profile object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Arcs2d As Arcs2d
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1)).Arcs2d
    'Create an arc
    Call objArcs.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0.05, yStart:=0, xEnd:=0, yEnd:=0.05)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
End Sub
See Also

Profile Object  | Profile Members