Application | Returns the active application object. |
Arcs2d | Returns the Arcs2d collection object for the referenced Profile object. |
AreaPropertiesCollection | |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Balloons | Returns the Balloons collection. |
Boundaries2d | Returns the Boundaries2d collection object for the referenced object. |
BSplineCurves2d | Returns the BSplineCurves2d collection object for the referenced Profile object. |
Circles2d | Returns the Circles2d collection object for the referenced Profile object. |
CircularPatterns2d | Returns the CircularPatterns2d collection object for the referenced Profile object. |
ComponentImages2d | |
CornerAnnotations | Returns the CornerAnnotations collection. |
CurveBody | Returns the CurveBody object associated with the referenced Curve, CurvePath, or Profile object. |
DatumFrames | Returns the DatumFrames collection. |
DatumPoints | Returns the DatumPoints collection. |
DatumTargets | Returns the DatumTargets collection. |
Dimensions | Returns the Dimensions collection object for the referenced Profile object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
DrawingObjects | Returns the DrawingObjects collection object for the referenced Profile object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Ellipses2d | Returns the Ellipses2d collection object for the referenced Profile object. |
EllipticalArcs2d | Returns the EllipticalArcs2d collection object for the referenced Profile object. |
FeatureControlFrames | Returns the FeatureControlFrames collection. |
Form | Returns the closure state of the referenced profile. |
GostWeldSymbols | Returns the GostWeldSymbols collection. |
Holes2d | Returns the Holes2d collection object for the referenced Profile object. |
Images2d | Returns the Images2d collection. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Leaders | Returns the Leaders collection. |
Lines2d | Returns the Lines2d collection object for the referenced Profile object. |
MountingBoss2dCollection | Returns the MountingBoss2dCollection collection. |
Nail | Returns the Nail associated with the feature profile. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
Points2d | Returns the Points2d collection object for the referenced Profile object. |
RectangularPatterns2d | Returns the RectangularPatterns2d collection object for the referenced Profile object. |
Relations2d | Returns the Relations2d collection object for the referenced Profile object. |
RolledBack | Specifies whether or not the feature associated with the referenced Profile object has been rolled back. |
Size | Returns the number of elements that are contained in the wireframe geometry of the referenced profile. |
SurfaceFinishSymbols | Returns the SurfaceFinishSymbols collection. |
SystemName | This read-only String property returns the system name for the referenced object. |
TextProfiles | Returns the TextProfiles collection object for the referenced object. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |
WeldSymbols | Returns the WeldSymbols collection. |