Solid Edge Part Type Library
BSplineCurves2d Property
Description
Returns the BSplineCurves2d collection object for the referenced Profile object.
Property type
Read-only property
Syntax
Visual Basic
Public Property BSplineCurves2d As BSplineCurves2d
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBSplns As SolidEdgeFrameworkSupport.BSplineCurves2d
    Dim MyArray(9) As Double
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If

    'define an array of points
    MyArray(0) = 0
    MyArray(1) = 0
    MyArray(2) = 0.03
    MyArray(3) = 0.02
    MyArray(4) = 0.04
    MyArray(5) = 0.01
    MyArray(6) = 0.05
    MyArray(7) = 0.08
    MyArray(8) = 0.07
    MyArray(9) = 0.04
    'Create an BSpline Curves collection object
    Set objBSplns = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1)).BSplineCurves2d
    'Create an BSpline curve object
    Call objBSplns.AddByPoints(Order:=9, ArraySize:=5, Array:=MyArray())
    ' USER DISPLAY

    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBSplns = Nothing
End Sub
See Also

Profile Object  | Profile Members