Solid Edge Part Type Library
EllipticalArcs2d Property
Description
Returns the EllipticalArcs2d collection object for the referenced Profile object.
Property type
Read-only property
Syntax
Visual Basic
Public Property EllipticalArcs2d As EllipticalArcs2d
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim start As Double
    Dim finish As Double
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create a Ellipses 2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an Ellipse object
    start = 180 * PI / 180
    finish = 230 * PI / 180
    Call objEllpArcs.AddByCenter(xCenter:=0.2, yCenter:=0.2, xMajorAxis:=0.5, yMajorAxis:=0.12, Ratio:=0.5, _
                                 Orientation:=igGeom2dOrientClockwise, StartAngle:=start, EndAngle:=finish)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc = Nothing
End Sub
See Also

Profile Object  | Profile Members