Solid Edge Part Type Library
IsAttributeSetPresent Property
Description
Returns True if a specified Attribute Set exists on the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsAttributeSetPresent( _
   ByVal Name As String _
) As Boolean
Parameters
Name
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfiles As SolidEdgeFrameworkSupport.Arcs2d
    Dim objProfile As SolidEdgeFrameworkSupport.Arc2d
    Dim objAttributeSets As Object
    Dim bAttribSetPresent As Boolean
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Create an profiles object
    Set objProfiles = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1)).Arcs2d
    'Create an profile
    Set objProfile = objProfiles.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0.05, yStart:=0, xEnd:=0, yEnd:=0.05)
    ' Get the AttributeSets collection object
    Set objAttributeSets = objProfile.AttributeSets
    'Create an AttributeSet
    Call objAttributeSets.Add("MyAttribSet")
    'Check for the presence of created Attributeset
    bAttribSetPresent = objProfile.IsAttributeSetPresent("MyAttribSet")
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfiles = Nothing
    Set objProfile = Nothing
    Set objAttributeSets = Nothing
End Sub
See Also

Profile Object  | Profile Members