Solid Edge Part Type Library
ProjectEdge Method
Specifies the Edge object to be projected.
Description
Projects a specified Edge onto the Profile plane, and returns a 2D geometry object that represents the projection.
Syntax
Visual Basic
Public Function ProjectEdge( _
   ByVal EdgeToProject As Object _
) As Object
Parameters
EdgeToProject
Specifies the Edge object to be projected.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objProfileset As SolidEdgePart.ProfileSet
    Dim objEdges As Object
    Dim objEdge As Object
    Dim objGeom2d As Object
    Dim objPrjGeom2d As Object
    ' Local variables to be declared here
    Const TESTFILE = "T:\vbtests\testcases\Cylinder.par"
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Close the existing Document
    Call objDoc.Close(Savechanges:=False)
    'Open the test case
    Set objDoc = objApp.Documents.Open(Filename:=TESTFILE)
    'Get the Edges collection of the ExtrudedProtrusion1
    Set objEdges = objDoc.Models(1).ExtrudedProtrusions(1).Edges(igQueryAll)
    'Get the circular edge
    Set objEdge = objEdges(1)
    'Get the ProfileSet
    Set objProfileset = objDoc.ProfileSets.Add
    'Add a Profile
    Set objProfile = objProfileset.Profiles.Add(objDoc.RefPlanes(1))
    'Project the Circular Edge onto the Profile to get the 2d Geometry object
    Set objPrjGeom2d = objProfile.ProjectEdge(objEdge)
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfileset = Nothing
    Set objProfile = Nothing
    Set objEdges = Nothing
    Set objEdge = Nothing
    Set objPrjGeom2d = Nothing
End Sub
See Also

Profile Object  | Profile Members