Solid Edge Part Type Library
SetAxisOfRevolution Method
Specifies the Axis of Revolution.
Description
Associates the axis of revolution with the profile.
Syntax
Visual Basic
Public Function SetAxisOfRevolution( _
   ByVal LineForAxis As Object _
) As Object
Parameters
LineForAxis
Specifies the Axis of Revolution.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim objProfile As SolidEdgePart.Profile
    Dim objRefAxis As SolidEdgePart.RefAxis
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create a Profile object
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Call objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.1)
    'Create a Line object
    Set objLine = objProfile.Lines2d.AddBy2Points(x1:=0, y1:=0, x2:=1, y2:=0)
    ' Set it as Axis of Revolution
    Set objRefAxis = objProfile.SetAxisOfRevolution(LineForAxis:=objLine)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLine = Nothing
    Set objProfile = Nothing
    Set objRefAxis = Nothing
End Sub
See Also

Profile Object  | Profile Members