StructureEditor Namespace
CreateRootNewItem Method
Description
This API is used to create root new empty item.
Syntax
Visual Basic
Public Function CreateRootNewItem() As Long
Remarks
In order to create new root item there should not be any file open in the Structure Editor application.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As StructureEditor.Application = Nothing
        Dim objStructureEditor As StructureEditor.SEECStructureEditor = Nothing
        Dim strUserName As String
        Dim strPassword As String
        Dim strGroup As String
        Dim strRole As String
        Dim strURL As String


        Try
            OleMessageFilter.Register()

            ' Start structure editor application
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("StructureEditor.Application"))
            objStructureEditor = objApplication.SEECStructureEditor
            objApplication.Visible = True

            strUserName = "Username"
            strPassword = ""
            strGroup = ""
            strRole = ""
            strURL = "http://Servername:8085/tc"

            If objStructureEditor.ValidateLogin(strUserName, strPassword, strGroup, strRole, strURL) = 0 Then
                objStructureEditor.CreateRootNewItem()
            End If
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            If Not objApplication Is Nothing Then
                ' Kill the instance of structure editor created
                objApplication.Quit()
            End If

            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

SEECStructureEditor Object  | SEECStructureEditor Members  | Solid Edge ST3 - What's New