StructureEditor Namespace
SEECStructureEditor Object Members
Overview 
Public Methods
Public Method AddExistingItemThis API is used to add the given Item into specified item.
Public Method AddItemInMultipleFiles 
Public Method AddItemToGivenProjectsThis API is used to add the Item to given projects.
Public Method AddNewItemThis API is used to add the new empty item into specified item.
Public Method AssignAllThis API is used to automatically assign system generated values to the mandatory properties of a document like item id,item revision,item name and dataset name.
Public Method ClearAllActionsThis API is used to clear the action, if any set on the solid edge file.
Public Method CloseThis API is used to close the solid edge file.
Public Method CreateRootNewItemThis API is used to create root new empty item.
Public Method GetProjectsForGivenItemIDThis API is used to get the projects for GivenItemID.
Public Method GetProjectsForLoggedInUserThis API is used to get the projects for logged in User.
Public Method OpenThis API is used to open a solid edge file from the teamcenter server into structure editor.
Public Method PerformActionsThis API is used to perform actions set on the solid edge file.
Public Method RemoveItemThis API is used to remove the given Item from specified item.
Public Method SetReplaceSelectedThis API is used to replace the existing item with new item.
Public Method SetReviseAllThis API is used to set revise action on all open solid edge files in structure editor.
Public Method SetReviseSelectedThis API is used to set revise action on a selected file in the structure editor.
Public Method SetSaveAsAllThis API is used to set save as action on all the open files in the structure editor.
Public Method SetSaveAsSelectedThis API is used to set save as action on a selected solid edge file in the structure editor.
Public Method SetSaveAsSpecificOccurrence 
Public Method ValidateLoginThis API is used to login to teamcenter server.
See Also

SEECStructureEditor Object