StructureEditor Namespace
SetReviseAll Method
Description
This API is used to set revise action on all open solid edge files in structure editor.
Syntax
Visual Basic
Public Function SetReviseAll() As Long
Remarks
Call this API after calling open() API. Because for calling this API a solid edge file needs to be opened in the structure editor application. If the action is set without opening a solid edge file in the application then nothing will happen.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As StructureEditor.Application = Nothing
        Dim objStructureEditor As StructureEditor.SEECStructureEditor = Nothing
        Dim strItemId As String
        Dim strItemRev As String
        Dim strFileName As String
        Dim strRevisionRule As String
        Dim strFolderName As String

        Try
            OleMessageFilter.Register()

            ' Start structure editor application
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("StructureEditor.Application"))
            objStructureEditor = objApplication.SEECStructureEditor
            objApplication.Visible = True

            strItemId = "081691"
            strItemRev = "A"
            strFileName = "a.asm"
            strRevisionRule = "Latest Working"
            strFolderName = ""

            If objStructureEditor.Open(strItemId, strItemRev, strFileName, strRevisionRule, strFolderName) = 0 Then
                objStructureEditor.SetReviseAll()
            End If
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            If Not objApplication Is Nothing Then
                ' Kill the instance of structure editor created
                objApplication.Quit()
            End If

            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

SEECStructureEditor Object  | SEECStructureEditor Members