Solid Edge Framework Type Library
ISEAddIn Object
Members 
Description
A control that represents a command added to Solid Edge through the AddIn interface.
Object Model
ISEAddIn ObjectCommandBarButton ObjectCommandBarButtonEvents ObjectCommandBar ObjectAddInEvents Object
Remarks
Addins written for V20 or later, it is prefered to implement the ISEAddInEx interface rather than the ISEAddIn interface.
See Also

ISEAddIn Members

Send comments on this topic.