Solid Edge Framework Type Library
ISEAddInEx Object
Members 
Description
A control that represents a command added to Solid Edge through the AddIn interface.
Object Model
ISEAddInEx ObjectAddInEdgeBarEvents Object
Remarks

Addins written for V20 or later, it is prefered to implement this interface rather than ISEAddIn.

A very important reason for this new interface is the lone method, SetAddInInfoEx that takes in a resource module filename as opposed to a module handle. This allows an addin to transmit resources to Edge for both 32 and 64 bit versions of edge. A failure to use the new interface will cause issues on 64 bit edge.

See Also

ISEAddInEx Members  | Solid Edge V20 - What's New

Send comments on this topic.