Sets and returns the ratio of the width of the window sheet tabs to the width of the window horizontal scrollbar.
Property type
Read-write property
Syntax
Visual Basic
Public Property SheetTabRatio As Double
Remarks
The default value is 0.75, meaning the sheet tabs are 3/4 the window width, while the horizontal scrollbar is 1/4 the window width). This property has no effect if either DisplayHScroll or DisplaySheetTabs is set to False. Its value is retained, but has no effect on the display.