Solid Edge Draft Type Library
UsableHeight Property
Collapse All
Expand All
Solid Edge Draft Type Library
>
SheetWindow Object
: UsableHeight Property
Description
Returns the height of the usable vertical space in the application window area.
Property type
Read-only property
Syntax
Visual Basic
Public Property UsableHeight As Integer
Remarks
The height is returned in points (1/72 inch). Adding sheet tabs, a horizontal scroll bar, or a toolbar reduces the usable height.
See Also
SheetWindow Object
|
SheetWindow Members