Solid Edge Assembly Type Library
Configurations Property
Description
Returns the Configurations collection object for the referenced AssemblyDocument object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Configurations As Configurations
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objAssemblyDocument As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objConfigurations As SolidEdgeAssembly.Configurations = Nothing
        Dim objConfiguration As SolidEdgeAssembly.Configuration = Nothing

        Try
            OleMessageFilter.Register()

            ' Start Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objAssemblyDocument = objApplication.ActiveDocument
            objConfigurations = objAssemblyDocument.Configurations

            ' Loop through configurations.
            For Each objConfiguration In objConfigurations

            Next
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

AssemblyDocument Object  | AssemblyDocument Members

Send comments on this topic.