| Solid Edge Assembly Type Library : AssemblyDocument Object | 
|  Activate | Makes the referenced object the active one. | 
|  ActivateAll | Activates all links in the referenced AssemblyDocument object. | 
|  AddMeasureVariable | Returns the measure variable object. | 
|  BindKeyToObject | Binds a specified reference key to a specified Occurrence, SubOccurrence, or TopologyReference object. | 
|  BreakAllInterpartLinks | |
|  BundleOccurrences | Creates a new file and places it in the assembly document with a grounded constraint at a position coincident with the assembly origin. | 
|  CheckInterference | Checks to see whether two selections share the same space. | 
|  CheckInterference2 | This method checks to see whether two selections share the same space. You can check one part against another part, or you can check one or more parts against themselves, against a second set of parts, or against all of the parts in the assembly. | 
|  Close | Closes the referenced object. | 
|  CopySketch | Copies the source layout or sketch into the target part or assembly either associatively or nonassociatively. | 
|  CreateFamilyFile | Creates a family of assemblies or alternate position assembly file with two members. | 
|  CreatePreview | |
|  CreateReference | Returns the Reference object created for the given ReferenceKey. | 
|  CreateReference2 | |
|  DeleteStructureCache | |
|  DisperseSubassembly | Moves the occurrences from the specified subassembly up one level. | 
|  EditProperties | Displays the EditProperties dialog box to allow the user to interactively set and view various properties of the referenced document object. | 
|  FreezeAllInterpartLinks | |
|  GenerateWireHarnessReport | |
|  GenerateWireReport | Generates a wire report for the referenced object. | 
|  GetBaseStyle | This method gets the base style for the referenced document object. | 
|  GetCapturedRelationshipInformation | |
|  GetContainerDocumentAndMatrixOfIPADoc | Returns the container document and transform matrix for an in-place-active document. | 
|  GetContainerDocumentAndOccurrenceOfIPADoc | |
|  GetGlobalParameter | Returns the setting of a specified global parameter for the referenced Application or document object. | 
|  GetInContextAssemblyNameForInterpartLinks | |
|  GetTopDocumentAndSubOccurrenceOfIPADoc | |
|  GoalSeek | |
|  HasInterpartLinks | |
|  ImportStyles | Imports the face styles from the given filename into the referenced document. If the optional variable Overwrite is true, styles with duplicate names will be overwritten. | 
|  ImportStyles2 | Copies styles of the specified type from the specified document. If bReplace is False, only styles that do not already exist will be copied. | 
|  MeasureAngle | Measures the sharp angle between lines or planes or keypoints. | 
|  MinimumDistance | Measures the minimum distance between two elements. | 
|  NewNavigatorWindow | creates a Pathfinder window for the referenced AssemblyDocument object. | 
|  NewWindow | Creates a new window that contains the referenced document. | 
|  NormalDistance | Measures the normal distance between lines or planes. | 
|  PMI_ByModelState | Get PMI dimensions and annotations by model state. Returns failure for invalid states. | 
|  PrintOut | Prints the contents of the referenced object. | 
|  PublishVirtualComponents | Publishes the virtual components for the referenced AssemblyDocument object. | 
|  Range | |
|  ReplaceComponents | |
|  RotateMultipleOccurrences | This method rotates the input occurrences. It takes input and returns an array of the occurrences that were moved or copied. If an occurrence was moved, the output occurrences are the same as the input occurrences. If an occurrence was copied, the output occurrences will be the new occurrence copies. | 
|  Save | Saves the referenced object. | 
|  SaveAs | Saves the referenced document to a new name, directory, or format. | 
|  SaveAsJT | Saves the referenced document to JT format with specified options. | 
|  SaveCopyAs | Saves a copy of the referenced document to a file without modifying the open document. | 
|  SaveModelAs | |
|  SeekReadOnlyAccess | |
|  SeekWriteAccess | Seeks write access to the document if it is available. | 
|  SendMail | Distributes the referenced document using the installed electronic mail system. | 
|  SetBaseStyle | This method sets the base style for the referenced document object. | 
|  SetGlobalParameter | Sets the value of a specified global parameter for the referenced Application or document object. | 
|  ThawAllInterpartLinks | |
|  TransferOccurrences | Transfers occurrences to a different subassembly. | 
|  TranslateMultipleOccurrences | This method translates the input occurrences. It takes input and returns an array of the occurrences that were moved or copied. If an occurrence was moved, the output occurrences are the same as the input occurrences. If an occurrence was copied, the output occurrences will be the new occurrence copies. | 
|  UpdateAll | Updates all links in the referenced AssemblyDocument object. | 
|  UpdateDocument | This method saves the document and its dependent documents and also all the modified documents in the referenced AssemblyDocument object. | 
|  UpdatePathfinder | This method provides automation functionality to update the assembly pathfinder by either refreshing the icons for each existing entry or by completely rebuilding the pathfinder. | 
|  UpdateStructureCache | 
|  ActiveSketch | Returns the active Sketch object. | 
|  AddInsStorage | Returns an IUnknown pointer to the object that implements the IStorage corresponding to the add-in substorage for the referenced object. | 
|  Application | Returns the active application object. | 
|  ArcSegments | Returns the ArcSegments collection object for the referenced AssemblyDocument object. | 
|  AsmRefPlanes | Returns the AsmRefPlanes collection object. | 
|  AssemblyBodies | |
|  AssemblyCopies | |
|  AssemblyDrivenPartFeatures | |
|  AssemblyFamilyEvents | |
|  AssemblyFamilyMembers | Returns the AssemblyFamilyMembers collection object. | 
|  AssemblyFeatures | |
|  AssemblyGroups | |
|  AssemblyMirrors | |
|  AssemblyPatterns | Returns the AssemblyPatterns collection. | 
|  AssemblyProperties | Returns the AssemblyProperties collection. | 
|  AssemblyRecomputeEvents | Fires assembly recompute events. | 
|  AttributeQuery | Returns the AttributeQuery object. | 
|  CapturedRelationshipCount | |
|  ComponentLayouts | |
|  Configurations | Returns the Configurations collection object for the referenced AssemblyDocument object. | 
|  Constructions | |
|  CoordinateSystems | Represents a collection of CoordinateSystem objects. | 
|  CreatedVersion | Returns the version of Solid Edge that was used to create the referenced document. | 
|  CurveSegments | Returns the CurveSegments collection object for the referenced AssemblyDocument object. | 
|  CutawaysCount | Returns the number of cutaway views associated with the referenced AssemblyDocument object. | 
|  DimensionStyles | Returns the DimensionStyles collection object for the referenced document. | 
|  Dirty | Specifies whether or not the referenced document has been modified since the last time it was saved. | 
|  DisplayName | Display Name - includes member name for FOA assembly documents | 
|  DocumentEvents | Returns the DocumentEvents object for the referenced document object. | 
|  ExplosionsCount | Returns the number of exploded views associated with the referenced AssemblyDocument object. | 
|  FaceStyles | Returns the FaceStyles collection object for the referenced document. | 
|  FastenerSystems | Represents Fastener Systems. | 
|  FillStyles | Returns the FillStyles collection object for the referenced document. | 
|  FullName | Returns the name and path of the referenced object. | 
|  GeometricVersion | Retrieves the geometric version number of the assembly document. | 
|  Harnesses | |
|  HasCapturedRelationships | |
|  HatchPatternStyles | Returns the HatchPatternStyles collection object for the referenced document. | 
|  HidePreviousLevel | This read-write Boolean property sets and returns whether the Hide Previous Level command is active for the referenced AssemblyDocument object. | 
|  HighlightSets | Returns the HighlightSets collection object for the referenced document object. | 
|  HoleDataCollection | Returns the HoleDataCollection object for the referenced document object. | 
|  InPlaceActivated | Specifies whether or not the referenced document is in-place activated. | 
|  InterpartLinks | |
|  IsAssemblySimplified | |
|  IsFileAlternatePositionByDocument | |
|  IsFileFamilyByDocument | Specifies whether the referenced document is a family of assembly file. | 
|  IsGeometricVersionDirty | Retrieves whether the geometric version number of the assembly document is dirty or not. | 
|  IsMultiCADDriven | |
|  IsSimplifyStateActive | |
|  IsTemplate | Specifies whether or not the referenced document is a template. | 
|  ItemNumbers | |
|  LabelWeldDataCollection | |
|  LastSavedVersion | Returns the version of Solid Edge that was used the last time the referenced document was saved. | 
|  Layers | Returns the Layers collection object. | 
|  Layouts | Returns the Layouts collection object on the Assembly document. | 
|  LinearStyles | Returns the LinearStyles collection object for the referenced document. | 
|  LineSegments | Returns the LineSegments collection object for the referenced AssemblyDocument object. | 
|  Name | Returns the name of the referenced object. | 
|  Occurrences | Returns the Occurrences collection object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Path | Returns the directory path name of the referenced document. | 
|  Paths | Returns the Keypoint Curves collection object for the referenced AssemblyDocument object. | 
|  PhysicalProperties | Returns the PhysicalProperties object for the referenced document. | 
|  Pipes | |
|  ProfileUndoSteps | This read-write Long property sets and returns the number of profile undo steps for the referenced document object. | 
|  Properties | For document objects, returns the PropertiesCollection colletion object. For Variables, sets and returns the variable properties. | 
|  Queries | Returns the Queries collection object for the referenced AssemblyDocument object. | 
|  ReadOnly | Specifies whether or not the referenced document has been opened as read-only. | 
|  Relations3d | Returns a collection of Relations3d objects for the referenced Part. | 
|  RelationshipsSelectSet | Returns the SelectSet object for the referenced AssemblyDocument object. | 
|  RootStorage | Returns the IUnknown pointer to the object implementing the root storage of the referenced document. | 
|  RoutingSlip | Returns the RoutingSlip object for the referenced document. | 
|  SectionViews | |
|  SegmentRelations3d | Returns the SegmentRelations3d collection object for the referenced AssemblyDocument object. | 
|  Segments | Returns the Segments collection object for the referenced AssemblyDocument object. | 
|  SelectSet | Returns the current selection set for the referenced document. | 
|  Sensors | Returns the Sensors collection object for the referenced document object. | 
|  SimplifiedAssemblies | Returns the collection of simplified Assemblies | 
|  Status | Returns the status of the specified object. | 
|  StructuralFrames | |
|  StudyOwner | Get Study Owner | 
|  SummaryInfo | Returns a SheetSummaryInfo object to provide access to descriptive properties for the referenced document. | 
|  Type | Specifies the type of the object being referenced. | 
|  UndoSteps | This read-write Long property sets and returns the number of undo steps for the referenced document object. | 
|  UnitsOfMeasure | Returns the UnitsOfMeasure object for the referenced document. | 
|  Variables | Returns the Variables collection object for the referenced document. | 
|  ViewStyles | Returns the ViewStyles collection object for the referenced document. | 
|  VirtualComponentOccurrences | Returns the VirtualComponentOccurrences collection object for the referenced AssemblyDocument object. | 
|  WeldmentAssembly | |
|  WeldmentAssemblyBeadDensity | |
|  WeldmentAssemblyBeadMaterial | |
|  Windows | Returns the Windows collection object. | 
|  WirePaths | Returns the WirePaths collection. | 
|  WireRuns | Returns the WireRuns collection. | 
|  Zones |