| Solid Edge Assembly Type Library > AssemblyDocument Object : PMI_ByModelState Method | 
| Visual Basic | 
|---|
| Public Sub PMI_ByModelState( _ ByRef PMIObj As Object, _ Optional ByVal PMIModelState As PMIModelStateConstants = 0 _ ) | 
| Value | Description | 
|---|---|
| seDesignModelState | Specifies the DESIGN model state - default value when getting PMI dimensions and annotations through the function PMI_ByModelState() | 
| seFlatModelState | Specifies the FLAT model state - will be used to get PMI dimensions and annotations based on flat model state through the function PMI_ByModelState() | 
| seSimplifyModelState | Specifies the SIMPLIFY model state - will be used to get PMI dimensions and annotations based on simplify model state through the function PMI_ByModelState() |