Solid Edge Assembly Type Library
Windows Property
Description
Returns the Windows collection object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Windows As Windows
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objWindows As SolidEdgeFramework.Windows
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Windows collection object using Windows property
    Set objWindows = objDoc.Windows
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objWindows = Nothing
End Sub
See Also

AssemblyDocument Object  | AssemblyDocument Members

Send comments on this topic.