| Solid Edge Assembly Type Library : AssemblyStitchWeld Object | 
|  AnnotationFormat | |
|  Application | |
|  BeadLength | |
|  EndOffset | Sets and returns the length of material to remove from the end of the weld bead for the referenced AssemblyStitchWeld object. | 
|  GapLength | Sets and returns the gap length between solid portions of the bead for the referenced StitchWeld object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | |
|  StartOffset | Sets and returns the length of material to remove from the start of the weld bead for the referenced AssemblyStitchWeld object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  Type | Specifies the type of the object being referenced. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |