Solid Edge Assembly Type Library
StartOffset Property
Description
Sets and returns the length of material to remove from the start of the weld bead for the referenced AssemblyStitchWeld object.
Property type
Read-write property
Syntax
Visual Basic
Public Property StartOffset As Double
Remarks
his property modifies the computed length of the bead, but does not modify the weld symbol attributes.
See Also

AssemblyStitchWeld Object  | AssemblyStitchWeld Members  | Solid Edge V18 - What's New

Send comments on this topic.