Solid Edge Assembly Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPhyProps As SolidEdgeAssembly.PhysicalProperties
    Dim objPhyPrApp As SolidEdgeFramework.Application
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Close the active document
    Call objDoc.Close
    ' opening an existing assembly file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Getting the PhysicalProperties object of the assembly document
    Set objPhyProps = objDoc.PhysicalProperties
    ' Getting the Application object of the PhysicalProperties object
    Set objPhyPrApp = objPhyProps.Application


    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPhyProps = Nothing
    Set objPhyPrApp = Nothing
End Sub
See Also

PhysicalProperties Object  | PhysicalProperties Members

Send comments on this topic.