Solid Edge Assembly Type Library
GetSelectSetPhysicalProperties Method
Returns the mass of the assembly.
Returns the volume of the assembly.
Returns the surface area of the assembly.
Returns the x-, y-, and z-coordinates of the center of gravity of the assembly.
Returns the x-, y-, and z-coordinates of the center of volume of the assembly, made with respect to the global origin.
Returns the lxx, lyy, lzz, lxy, lxz, and lyz components of the global moments of inertia.
Returns the orientation of the first principal axis.
Returns the orientation of the second principal axis.
Returns the orientation of the third principal axis.
Returns the lxx, lyy, and lzz components of the principal moments of inertia.
Returns three values that specify the radii of gyration.
Description
Returns the physical property calculations for the active select set.
Syntax
Visual Basic
Public Sub GetSelectSetPhysicalProperties( _
   ByRef Mass As Double, _
   ByRef Volume As Double, _
   ByRef Area As Double, _
   ByRef CenterOfMass() As Double, _
   ByRef CenterOfVolume() As Double, _
   ByRef GlobalMoments() As Double, _
   ByRef PrincipalAxis1() As Double, _
   ByRef PrincipalAxis2() As Double, _
   ByRef PrincipalAxis3() As Double, _
   ByRef PrincipalMoments() As Double, _
   ByRef RadiiOfGyration() As Double _
) 
Parameters
Mass
Returns the mass of the assembly.
Volume
Returns the volume of the assembly.
Area
Returns the surface area of the assembly.
CenterOfMass
Returns the x-, y-, and z-coordinates of the center of gravity of the assembly.
CenterOfVolume
Returns the x-, y-, and z-coordinates of the center of volume of the assembly, made with respect to the global origin.
GlobalMoments
Returns the lxx, lyy, lzz, lxy, lxz, and lyz components of the global moments of inertia.
PrincipalAxis1
Returns the orientation of the first principal axis.
PrincipalAxis2
Returns the orientation of the second principal axis.
PrincipalAxis3
Returns the orientation of the third principal axis.
PrincipalMoments
Returns the lxx, lyy, and lzz components of the principal moments of inertia.
RadiiOfGyration
Returns three values that specify the radii of gyration.
Remarks
If no parts or subassemblies are part of the selection set, the physical properties are computed for the entire assembly.
See Also

PhysicalProperties Object  | PhysicalProperties Members

Send comments on this topic.