Solid Edge Assembly Type Library
Update Method
Description
Updates the referenced object.
Syntax
Visual Basic
Public Sub Update() 
Remarks
Update re-computes the physical properties of an assembly to reflect the current configuration. These properties are computed with the current specified tolerance and density.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPhyProps As SolidEdgeAssembly.PhysicalProperties
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    Dim bBefUpDt As Boolean
    Dim bAftUpDt As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Close the active document
    Call objDoc.Close
    ' opening an existing assembly file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Getting the PhysicalProperties object of the assembly document
    Set objPhyProps = objDoc.PhysicalProperties
    'Getting the IsUpToDate property before update
    bBefUpDt = objPhyProps.IsUpToDate
    'Update the physicalproperties first and get the status
    Call objPhyProps.Update
    bAftUpDt = objPhyProps.IsUpToDate

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPhyProps = Nothing
End Sub
See Also

PhysicalProperties Object  | PhysicalProperties Members

Send comments on this topic.