Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeAssembly.AssemblyDocument
Dim objTangntRelation As SolidEdgeAssembly.TangentRelation3d
Dim objAttributeSets As Object
' Local variables to be declared here
Const TESTFILE = "T:\vbtests\testcases\TangntRel3d.asm"
Dim bAttribSetPresent As Boolean
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
On Error GoTo 0
objDoc.Close False
'Open an existing Assembly containing TangentRelation
Set objDoc = objApp.Documents.Open(Filename:=TESTFILE)
'Get hold of the TangentRelation from the Relations3d collection
Set objTangntRelation = objDoc.Relations3d(2)
'Get the AttributeSets collection object
Set objAttributeSets = objTangntRelation.AttributeSets
'Create an AttributeSet
objAttributeSets.Add "MyAttribSet"
'Check for the presence of the AttributeSet
bAttribSetPresent = objTangntRelation.IsAttributeSetPresent("MyAttribSet")
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objTangntRelation = Nothing
Set objAttributeSets = Nothing
End Sub