|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DetailedStatus | Returns the detailed status of the Relation3d object. | 
|  HalfSpacePositive | Indicates whether the referenced TangentRelation3d is placed on the positive normal side of a plane (True) or the reverse normal side of a plane (False). | 
|  Index | Returns the numeric index for the active object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Occurrence1 | Returns the first Occurrence object for the referenced relationship object. | 
|  Occurrence2 | Returns the second Occurrence object for the referenced relationship object. | 
|  Offset | Sets or returns the distance (in working units) that two parts are offset from one another. | 
|  Parent | Returns the parent object for the referenced object. | 
|  RangedOffset |  | 
|  RangeHigh |  | 
|  RangeLow |  | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  Type | Specifies the type of the object being referenced. |