Solid Edge Assembly Type Library
Offset Property
Description
Sets or returns the distance (in working units) that two parts are offset from one another.
Property type
Read-write property
Syntax
Visual Basic
Public Property Offset As Double
Remarks
If the parts are aligned, the Offset property can be either a positive or a negative value. If the parts are mated, the Offset property can only be a positive value.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objTangntRelation As SolidEdgeAssembly.TangentRelation3d
    ' Local variables to be declared here
    Const TESTFILE = "T:\vbtests\testcases\TangntRel3d.asm"
    Dim dblOffset As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    objDoc.Close False
    'Open an existing Assembly containing TangentRelation
    Set objDoc = objApp.Documents.Open(Filename:=TESTFILE)
    'Get hold of the TangentRelation from the Relations3d collection
    Set objTangntRelation = objDoc.Relations3d(2)
    'Get the Offset value of this TangentRelation
    dblOffset = objTangntRelation.Offset
    'Change the Offset value
    objTangntRelation.Offset = 0.05
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objTangntRelation = Nothing
End Sub
See Also

TangentRelation3d Object  | TangentRelation3d Members

Send comments on this topic.