Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objArc2 As SolidEdgeFrameworkSupport.Arc2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create an arc
    Set objArc1 = objArcs.AddByCenterStartEnd(xStart:=-0.05, yStart:=0, xCenter:=0, _
                                              yCenter:=0, xEnd:=0.05, yEnd:=0)
    ' Create another Arc object
    Set objArc2 = objArcs.AddByCenterStartEnd(xStart:=0, yStart:=0, xCenter:=0, _
                                              yCenter:=0.05, xEnd:=0, yEnd:=0.1)
    ' CornerTrim the Arcs
    Call objArc1.CornerTrim(xKeep:=0, yKeep:=0.05, TargetObj:=objArc2, xTargetKeep:=0, _
                            yTargetKeep:=0.1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objArc1 = Nothing
    Set objArc2 = Nothing
End Sub