Solid Edge FrameworkSupport Type Library
Arc2d Object Members
Overview 
Public Methods
Public Method AddSegmentedStyleDefines a segment on a graphic object and assigns a linear style to that segment.
Public Method BringForwardChanges the display order of the referenced object by moving it in front of the first object that obscures it.
Public Method BringToFrontChanges the display order of the referenced object by moving it in front of all other overlapping objects.
Public Method CopyPlaces a copy of the referenced object on the clipboard.
Public Method CornerTrimTrims or extends the referenced object and a target object to intersect.
Public Method CutMoves the referenced object to the system clipboard.
Public Method DeleteDeletes the referenced object.
Public Method DuplicateCopies the referenced object to a specified location, creating a new instance of the object with the same property values as the original.
Public Method ExtendExtends open graphic elements to a specified location.
Public Method GetCenterPointReturns the point that is the center of the referenced object.
Public Method GetEndPointReturns the coordinates of the end point of the referenced object.
Public Method GetKeyPointReturns information about a specified key point.
Public Method GetMajorAxisReturns the coordinates of the major axis vector for the referenced object.
Public Method GetSegmentedStyleReturns the start point, end point, and linear style applied to a specified segment of a 2-D geometry object.
Public Method GetStartPointReturns the coordinates of the start point for the referenced object.
Public Method MirrorCopies the referenced object about an axis.
Public Method MoveMoves the referenced object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method RemoveAllSegmentedStylesRemoves all segments defined for the referenced graphic object.
Public Method RemoveSegmentedStyleRemoves the segmented style at the specified index on the graphic.
Public Method RotateRotates the referenced object about the point specified by the angle in radians.
Public Method ScaleScales the referenced object by a specified factor.
Public Method SelectSelects the referenced object in the active window.
Public Method SendBackwardChanges the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Public Method SendToBackChanges the display order of visible objects by moving the referenced object behind all overlapping objects.
Public Method SetCenterPointRelocates the center point of the specified object.
Public Method SetEndPointSets the x and y values of the end point for the referenced object.
Public Method SetKeyPointSets the position for a specified key point.
Public Method SetMajorAxisSets the x and y values of the major axis vector for the referenced object.
Public Method SetSegmentedStyleApplies a new linear style to a specified segment on a graphic object.
Public Method SetStartPointRelocates the starting point of the referenced object.
Public Method SplitAtPointThis method splits the referenced object at the split point specified. For closed BSplineCurve2d objects, you must use the SplitAtPoints method.
Public Method TrimDeletes sections of geometry that intersect other objects.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DocumentReturns the document to which the referenced object belongs.
Public Property FilletReturns the FilletGeometry2d object associated with the referenced Arc2d object.
Public Property IndexReturns the numeric index for the active object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property IsFilletSpecifies whether or not the referenced Arc2d object is a fillet.
Public Property KeyReturns a key (a string) to find the object relative to its owning parents.
Public Property KeyPointCountReturns the number of keypoints/handles that are supported by the referenced object.
Public Property LayerSets and returns the named layer on which the referenced object resides.
Public Property LengthSpecifies the length of the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property OrientationSets and returns the direction in which an arc or elliptical arc is drawn.
Public Property ParentReturns the parent object for the referenced object.
Public Property RadiusReturns the radius of the referenced object.
Public Property RelationshipsReturns a collection of objects that are related to the referenced graphic object.
Public Property SegmentedStyleCountReturns the number of segmented styles defined for the referenced graphic object.
Public Property ShowCurvatureCombShows the curvature comb for the referenced object.
Public Property StartAngleSets and returns the angle, in radians, at which the arc begins along a circle or ellipse with regard to the major axis.
Public Property StyleFor collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Public Property SweepAngleSets and returns the angle, in radians, at which the arc ends along a circle or ellipse with regard to the major axis of the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
Public Property ZOrderSpecifies the front-to-back order in which an object is displayed relative to other objects.
See Also

Arc2d Object

Send comments on this topic.