Solid Edge FrameworkSupport Type Library
Orientation Property
Description
Sets and returns the direction in which an arc or elliptical arc is drawn.
Property type
Read-write property
Syntax
Visual Basic
Public Property Orientation As Geom2dOrientationConstants
Remarks
This direction is in respect to the major axis and is either clockwise or counterclockwise. Valid values are members of the Geom2dOrientationConstants constant set.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim cOrntn As Geom2dOrientationConstants
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create an arc
    Set objArc1 = objArcs.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0.05, _
                                              yStart:=0, xEnd:=0, yEnd:=0.05)
    ' Get the Orientation of the Arc object
    cOrntn = objArc1.Orientation
    objArc1.Orientation = igGeom2dOrientClockwise
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objArc1 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members

Send comments on this topic.