Solid Edge FrameworkSupport Type Library
Relationships Property
Description
Returns a collection of objects that are related to the referenced graphic object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Relationships As Relationships2d
Remarks
A geometry object can be a member of any relation such as a parallel relation, a perpendicular relation, and so forth. To find all relations of which the geometry object is a member, return the Relationships collection object through the geometry object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
    Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
    Dim objL1 As SolidEdgeFrameworkSupport.Line2d
    Dim objL2 As SolidEdgeFrameworkSupport.Line2d
    Dim objRelns As SolidEdgeFrameworkSupport.Relationships2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an Arcs collection object
    Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
    ' Create two intersecting line objects
    Set objL1 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)). _
                Lines2d.AddBy2Points(x1:=0, y1:=0, x2:=0.1, y2:=0)
    Set objL2 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)). _
                Lines2d.AddBy2Points(x1:=0, y1:=0.1, x2:=0, y2:=0)
    ' Create an arc object
    Set objArc1 = objArcs.AddAsFillet(Obj1:=objL1, Obj2:=objL2, Radius:=0.05, _
                                      xDirection:=0.15, yDirection:=0.05)
    ' Get the Relationships of Arc object
    Set objRelns = objArc1.Relationships
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objArcs = Nothing
    Set objL1 = Nothing
    Set objL2 = Nothing
    Set objArc1 = Nothing
End Sub
See Also

Arc2d Object  | Arc2d Members

Send comments on this topic.