Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objArcs As SolidEdgeFrameworkSupport.Arcs2d
Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
Dim dblAng As Double
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Create an Arcs collection object
Set objArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Arcs2d
' Create an arc object
Set objArc1 = objArcs.AddByCenterStartEnd(xCenter:=0, yCenter:=0, xStart:=0.05, _
yStart:=0, xEnd:=0, yEnd:=0.05)
' Set the SweepAngle
dblAng = objArc1.SweepAngle
objArc1.SweepAngle = PI
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objArcs = Nothing
Set objArc1 = Nothing
End Sub