Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objArcs2d As SolidEdgeFrameworkSupport.Arcs2d
Dim objArc2d1 As SolidEdgeFrameworkSupport.Arc2d
Dim objArc2d2 As SolidEdgeFrameworkSupport.Arc2d
Dim lngZorder1 As Long
Dim lngZorder2 As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'create arcs2d object
Set objArcs2d = objSheet.Arcs2d
' Create an arc
Set objArc2d1 = objArcs2d.AddByStartAlongEnd(xStart:=0.233, yStart:=0.149, _
xAlong:=0.233, yAlong:=0.278, xEnd:=0.338, yEnd:=0.324)
'Get zorder for the arc
lngZorder1 = objArc2d1.ZOrder
'Create another Arc object
Set objArc2d2 = objArcs2d.AddByStartAlongEnd(xStart:=0.325, yStart:=0.16, _
xAlong:=0.269, yAlong:=0.293, xEnd:=0.158, yEnd:=0.34)
lngZorder2 = objArc2d2.ZOrder
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objArcs2d = Nothing
Set objArc2d1 = Nothing
Set objArc2d2 = Nothing
End Sub