Solid Edge FrameworkSupport Type Library
GetSegmentedStyle Method
Specifies the index of the segmented style to return.
Coordinates for the start of the segment.
Coordinates for the start of the segment.
Coordinates for the end of the segment.
Coordinates for the end of the segment.
LinearStyle object applied to the segment.
Description
Returns the start point, end point, and linear style applied to a specified segment of a 2-D geometry object.
Syntax
Visual Basic
Public Sub GetSegmentedStyle( _
   ByVal Index As Long, _
   ByRef x1 As Double, _
   ByRef y1 As Double, _
   ByRef x2 As Double, _
   ByRef y2 As Double, _
   ByRef Style As Object _
) 
Parameters
Index
Specifies the index of the segmented style to return.
x1
Coordinates for the start of the segment.
y1
Coordinates for the start of the segment.
x2
Coordinates for the end of the segment.
y2
Coordinates for the end of the segment.
Style
LinearStyle object applied to the segment.
Remarks
The segment is specified by its index value.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objBSpln1 As SolidEdgeFrameworkSupport.BSplineCurve2d
    Dim objLinStyle1 As SolidEdgeFrameWork.LinearStyle
    Dim objLinStyle2 As SolidEdgeFrameWork.LinearStyle
    Dim MyArray(9) As Double
    Dim strStyleName As String, strStyleParent As String
    Dim dblX1 As Double, dblY1 As Double, dblX2 As Double, dblY2 As Double
    Dim objStyle As Object
    Dim lngIdx As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Define an Array of Points
    MyArray(0) = 0.05
    MyArray(1) = 0.05
    MyArray(2) = 0.09
    MyArray(3) = 0.12
    MyArray(4) = 0.14
    MyArray(5) = 0.05
    MyArray(6) = 0.19
    MyArray(7) = 0.18
    MyArray(8) = 0.25
    MyArray(9) = 0.09
    'Create a BSplineCurve object
    Set objBSpln1 = objSheet.BSplineCurves2d.AddByPoints(Order:=4, ArraySize:=5, _
                                                         Array:=MyArray())
    ' Create a LinearStyle2d Object
    strStyleName = "LinearStyleDotted"
    strStyleParent = "Dotted"
    Set objLinStyle1 = objDoc.LinearStyles.Add(Name:=strStyleName, _
                                               Parent:=strStyleParent)

    ' Add a SegmentedStyle to the BSplineCurve
    Call objBSpln1.AddSegmentedStyle(x1:=0.05, y1:=0.05, x2:=0.14, _
                                     y2:=0.05, Style:=objLinStyle1)
    ' Create a LinearStyle2d Object
    strStyleName = "LinearStyleDashed"
    strStyleParent = "Center"
    Set objLinStyle2 = objDoc.LinearStyles.Add(Name:=strStyleName, _
                                               Parent:=strStyleParent)
    ' Add a SegmentedStyle to the BSplineCurve
    Call objBSpln1.AddSegmentedStyle(x1:=0.14, y1:=0.05, x2:=0.19, _
                                     y2:=0.18, Style:=objLinStyle2)
    ' Add 3rd SegmentedStyle to the BSplineCurve
    Call objBSpln1.AddSegmentedStyle(x1:=0.19, y1:=0.18, x2:=0.25, _
                                     y2:=0.09, Style:=objLinStyle1)

    ' Get the SegmentedStyle
    Call objBSpln1.GetSegmentedStyle(Index:=2, x1:=dblX1, y1:=dblY1, _
                                     x2:=dblX2, y2:=dblY2, Style:=objStyle)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objBSpln1 = Nothing
    Set objLinStyle1 = Nothing
    Set objLinStyle2 = Nothing
End Sub
See Also

BSplineCurve2d Object  | BSplineCurve2d Members

Send comments on this topic.