AddSegmentedStyle | Defines a segment on a graphic object and assigns a linear style to that segment. |
BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
Copy | Places a copy of the referenced object on the clipboard. |
CornerTrim | Trims or extends the referenced object and a target object to intersect. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
DeleteNode | Removes a specified node from a BSplineCurve2d object. |
Duplicate | Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original. |
Evaluate | This method takes the input parameter location and returns the point, first derivative, second derivative, and curvature of the location for the referenced BSplineCurve2d object. |
Extend | Extends open graphic elements to a specified location. |
GetCentroid | Returns the coordinates of the centroid of the referenced object. |
GetClosestPoint | This method returns the point on the referenced BSplineCurve2d object that is closest to the input point. |
GetData | This method returns all basic data for the referenced BSplineCurve2d object. |
GetKeyPoint | Returns information about a specified key point. |
GetNearestNode | Returns the index of the node point that is closest to the specified coordinates on the referenced BSplineCurve2d object. |
GetNode | Returns the coordinates of a specified node on the referenced BSplineCurve2d object. |
GetParameterRange | This method returns the start and end parameters of the referenced BSplineCurve2d object. |
GetPole | Returns the x and y values of a pole on the referenced BSplineCurve at a specified index. |
GetSegmentedStyle | Returns the start point, end point, and linear style applied to a specified segment of a 2-D geometry object. |
InsertNodeAtPoint | This method places a node at a specified point on a BSplineCurve2d object. The point must lie on the curve. |
Mirror | Copies the referenced object about an axis. |
Move | Moves the referenced object. |
Range | Returns the high and low range values for the referenced object. |
RemoveAllSegmentedStyles | Removes all segments defined for the referenced graphic object. |
RemoveSegmentedStyle | Removes the segmented style at the specified index on the graphic. |
Reparameterize | This method calculates new parameters for the referenced BSplineCurve2d object. It attempts to space the parameters as evenly as possible in order to better define the curve. This can make downstream operations more robust. However, it can also change the shape of the curve. |
Rotate | Rotates the referenced object about the point specified by the angle in radians. |
Scale | Scales the referenced object by a specified factor. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetDegree | This method sets the degree of the referenced BSplineCurve2d object. |
SetKeyPoint | Sets the position for a specified key point. |
SetNode | Relocates an existing node on a BSplineCurve2d object. |
SetPole | Relocates one of the points that define the control polygon of the referenced BSplineCurve2d object. |
SetSegmentedStyle | Applies a new linear style to a specified segment on a graphic object. |
Simplify | This method simplifies the curve using the specified tolerance. This method usually results in a shape change and might also result in fewer control vertices and/or fewer edit points. It retains any endpoint constraints/dimensions and any connected Blue Dots, and deletes all other constraints/dimensions attached to the curve. |
SplitAtPoint | This method splits the referenced object at the split point specified. For closed BSplineCurve2d objects, you must use the SplitAtPoints method. |
SplitAtPoints | This method splits the referenced closed-curve object at the split points specified. For open BSplineCurve2d objects, you must use the SplitAtPoint method. |
Trim | Deletes sections of geometry that intersect other objects. |