Solid Edge FrameworkSupport Type Library
Mirror Method
Specifies the x coordinate of the first point on the mirror axis.
Specifies the y coordinate of the first point on the mirror axis.
Specifies the x coordinate of the second point on the mirror axis.
Specifies the y coordinate of the second point on the mirror axis.
Specifies whether or not the copied object will be active.
Description
Copies the referenced object about an axis.
Syntax
Visual Basic
Public Function Mirror( _
   ByVal x1 As Double, _
   ByVal y1 As Double, _
   ByVal x2 As Double, _
   ByVal y2 As Double, _
   Optional ByVal BooleanCopyFlag As Variant _
) As Object
Parameters
x1
Specifies the x coordinate of the first point on the mirror axis.
y1
Specifies the y coordinate of the first point on the mirror axis.
x2
Specifies the x coordinate of the second point on the mirror axis.
y2
Specifies the y coordinate of the second point on the mirror axis.
BooleanCopyFlag
Specifies whether or not the copied object will be active.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBSplns As SolidEdgeFrameworkSupport.BSplineCurves2d
    Dim objBSpln1 As SolidEdgeFrameworkSupport.BSplineCurve2d
    Dim MyArray(9) As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Define an Array of Points
    MyArray(0) = 0
    MyArray(1) = 0
    MyArray(2) = 0.03
    MyArray(3) = 0.02
    MyArray(4) = 0.04
    MyArray(5) = 0.01
    MyArray(6) = 0.05
    MyArray(7) = 0.08
    MyArray(8) = 0.07
    MyArray(9) = 0.04
    'Create a BSplineCurves collection object
    Set objBSplns = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                        objDoc.RefPlanes(1)).BSplineCurves2d

    'Create a BSplineCurve object
    Set objBSpln1 = objBSplns.AddByPoints(Order:=4, ArraySize:=5, Array:=MyArray())
    ' Create a Mirror of the object
    Call objBSpln1.Mirror(x1:=0, y1:=0, x2:=0.2, y2:=0)
    If objBSplns.Count <> 1 Then
        MsgBox ("Error in the Mirror method of BSplineCurve2d object ")
    End If
    ' Delete the object
    Call objBSpln1.Delete
    'Create a BSplineCurve object again
    Set objBSpln1 = objBSplns.AddByPoints(Order:=4, ArraySize:=5, Array:=MyArray())
    ' Create a Mirror of the object
    Call objBSpln1.Mirror(x1:=0, y1:=0, x2:=0.1, y2:=0, BooleanCopyFlag:=True)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBSplns = Nothing
    Set objBSpln1 = Nothing
End Sub
See Also

BSplineCurve2d Object  | BSplineCurve2d Members

Send comments on this topic.