AttributeSets | Returns the AttributeSets collection object for the referenced object. |
CustomSheetColor | Sets and returns the color of the sheet when the UseCustomSheetColor property is True. |
DynamicGridSpacing | Sets and returns the spacing definition for a dynamic grid. |
GridColor | Sets and returns the color of the grid for the referenced BackDrop object when the GridDisplay property is True. |
GridDisplay | Specifies whether or not the grid of the referenced BackDrop object is to be displayed. |
GridType | Sets and returns the type of the grid. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
MarginColor | Sets and returns the color of the margin of the referenced BackDrop object when the MarginDisplay property is True. |
MarginDisplay | Specifies whether or not the margin of the referenced BackDrop object is displayed in the window. |
StaticGridSpacing | Sets and returns the spacing of a static grid for the referenced BackDrop object. |
UseCustomSheetColor | Determines if a custom sheet color is to be used in the window as a backdrop color. |